cancel
Showing results for 
Search instead for 
Did you mean: 

USB FS VCP won't enumerate on pc STM32F412

SMaes.10
Associate

I'm using standard peripheral library and the ST provide USB OTG device/HOST lib.

My sysyclock is running on 60Mhz with PLL (HSE of 25MHz) and USB clock is 48MHz.

Everything compiles and I expect after calling the Init function that the comport should be found by my pc, but nothing happens. Has anyone an Idea where to start checking why it's not working? I suppose the lib itself should already configure peripheral clocks and enable them?

My own clock config is as described above.

A quick generated example with cube mx works on my board, but dfue to collaboration with another party I have to use the standard peripheral lib an can't use cube mx.

I tried to use the mprovide usb middle ware from the cubemx project in my project, than I get a not recognised usb device notification on my pc, but after initialisation of the usb lib, my stm controllers hangs up or clocks stoped

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0