cancel
Showing results for 
Search instead for 
Did you mean: 

USB disconnect performence

Barbie
Associate II
Posted on April 28, 2013 at 14:12

I have a problem when I use the USB in the Boot application and then jump to my main app without detach the USB . On the main I open it again but the other side lost connection in between. I try to stop the clock to the USB when I jump but no help.

Is there a simple way or a function that can do USB disconnect so the other side see it as the USB was disconnect?

Bar.

#usb-disconnect
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
tsuneo
Senior
Posted on April 29, 2013 at 15:42

http://www.keil.com/forum/22901/usb-soft-disconnect/