2020-06-24 12:21 AM
Hello,
I want to use a NUCLEO-L432KC as an interface card on a computer.
The L432KC reboots when it is plugged into the USB port of my computer in Windows 10.
These restarts occur randomly after a few minutes.
These restarts also occur if I supply it with 12V and it is connected to the USB port of the computer.
I did not observe these restarts when the L432KC is powered without being plugged into a USB port.
I did not observe these reboots when plugged into the USB port of another computer in Windows 7 and in Linux computer (Ubuntu 18.04).
Here is my test code:
#include "mbed.h"
DigitalOut myled (LED1);
DigitalIn button (PA_7);
int main () {
while (! button) {
myled = 1; // LED is ON
wait (1.0); // 1 seconde
myled = 0; // LED is OFF
wait (1.0);
}
while (1) {
myled = 1; // LED is ON
wait (0.25); // 250 ms
myled = 0; // LED is OFF
wait (0.25);
}
}A button is connected between PA_7 and + 5V, a restoring resistor (15kohm) between PA_7 and GND.
At startup (or restart) the LED flashes at 0.5 Hertz, after pressing the button connected to PA_7 the LED flashes at 2Hz.
If you have an idea on the origin of the problem ?
Marc.
2020-06-29 6:48 AM
Hello,
I answer my own post:
I first tried to update the ST-LINK driver
After that, I had to restart the computer, the operation was not yet stable (I had the impression that things were continuing to implement this in Windows 10).
I then installed the ST-LINK firmware update
After that, I restarted the computer again, the operation was still not stable (and I still had the impression that things continued to set it up).
I installed ST-LINK utility
Then I restart. It functioned. But I don't think the ST-LINK utility had anything to do with it. I thought rather that it was the update of the driver ST-LINK or the update of the firmware.
Marc.