cancel
Showing results for 
Search instead for 
Did you mean: 

STM32Fxxx MTP USB Device

bruce239955
Associate II
Posted on September 26, 2016 at 11:48

Does anyone know if ST supports the Media Transport Protocol (MTP) for a USB device as opposed to a USB Host?

For a lot of applications I'm sure this would be very useful addition, since it enables the USB device to retain control of its file system (e.g. where there is an external SD card connected), while still allowing a USB Host to be connected to view/read/write files.

I'm aware that there are stack vendors who can supply this feature, but the cost is very high.

Comments?

#usb #device #mtp
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
tsuneo
Senior
Posted on September 27, 2016 at 19:32

The original post was too long to process during our migration. Please click on the provided URL to read the original post. https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I6kZ&d=%2Fa%2F0X0000000bub%2F_fXmx8IUWNNQ42Ymrsb9qRZmIvU9aE6QH7PAZyr48jo&asPdf=false