cancel
Showing results for 
Search instead for 
Did you mean: 

stm32f407 USB HID device can miss a report from PC? - I think I need a little advice :)

daviddudas9
Associate
Posted on September 27, 2015 at 16:42

Hi all,

normally my application sends a report to the host PC when there's any change. The host PC sends 3 types of reports constantly to the device, and I have to answer immediately for one of theese message (with a second type of report). Everything seems fine, but after a couple of minutes something happens :)

With USBlyzer I can see PC issues an output report but my application running on STM32F4 doesn't process one report correctly? There is no

URB Bulk or Interrupt Transfer succeeded

Message in USBlyzer for that message and the application on the host PC side gets stuck. I tried to catch whitout much success. I'm sure it's not because a still processed ISR and it's not a HAL_PCD_IS_INVALID_INTERRUPT (the later is not a problem it seems, because I've some during normal operation). Any idea? Is it possible ISR misses it?

It seems this problem always happens when the 16byte long report comes from PC (however before the problem it arrives successfully several times). USBD_CUSTOMHID_OUTREPORT_BUF_SIZE is 16 byte in my code, but I'm not sure if it has any effect.

Thanks,

D

#otg #usb #interrupt
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0