STM32F4 USBX CDC-ACM Bulk IN endpoint Stall
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-04-25 1:03 PM - edited ‎2025-04-25 1:05 PM
I am looking for help solving a CDC-ACM problem with Azure Rtos ThreadX, and the USBX Middleware for STM32F4.
My device is an STM32F427VGTx.
I currently have a project that uses the USBX host library. I am connecting up to 4x CDC-ACM devices through an off-the-shelf USB Hub.
I had problems connecting multiple devices through the hub, but I have solved that after following the solution to update the USBX core bsp from the stm32-mw-usbx repo. (STM32H7 and USB2514 Continued Problems)
I can connect to all 4x CDC-ACM devices (data class instance and control class instance enumerate successfully on all devices).
I can send commands to all devices using the control interface by sending a transfer request to the control endpoint.
I can read from up to two CDC-ACM devices, but the third and fourth device will timeout after calling ux_host_class_cdc_acm_read. The function returns a transfer-request-timeout after failing to retrieve the ux_host_semaphore. The status of ux_host_semaphore_get is always TX_NO_INSTANCE and is set by tx_semaphore_cleanup() after semaphore timeout in a thread.
I am calling ux_host_class_cdc_acm_read inside a thread. It works for up to two devices. The first two still work while the third and fourth don't.
Solved! Go to Solution.
- Labels:
-
AzureRTOS
-
STM32F4 Series
-
USB
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-05-07 12:37 PM
I have resolved the problem by reducing the amount of endpoints used in each CDC-ACM device.
For anyone struggling with a similar problem, count how many endpoints you are using.
The STM32 USB Peripheral has up to 8 endpoints. After reducing to two endpoints each (BULK IN, CMD OUT) I am able to succesfully connect and communicate with 4 CDC-ACM devices.
Our CDC-ACM devices was built using STM32G4 and the initial example used 4 endpoints (BULK IN, BULK OUT, CMD OUT, ISOCHRONOUS). That was why I could only connect to two devices before.
Thank you @FBL for the advice.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-05-07 7:43 AM
Hi @akorsich
Are you interfacing low speed devices? You may need to check this limitation section 2.14.2 Host packet transmission may hang when connecting through a hub to a low-speed device.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-05-07 12:37 PM
I have resolved the problem by reducing the amount of endpoints used in each CDC-ACM device.
For anyone struggling with a similar problem, count how many endpoints you are using.
The STM32 USB Peripheral has up to 8 endpoints. After reducing to two endpoints each (BULK IN, CMD OUT) I am able to succesfully connect and communicate with 4 CDC-ACM devices.
Our CDC-ACM devices was built using STM32G4 and the initial example used 4 endpoints (BULK IN, BULK OUT, CMD OUT, ISOCHRONOUS). That was why I could only connect to two devices before.
Thank you @FBL for the advice.