cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F205RBT6 USB host example - for pendrive

embedded
Associate
Posted on March 10, 2014 at 06:07

Is there any example code on how to use it.

I have used sd card with fat32 format & created a test file.

Now when user conect external pen drive to system then I have to write that text file from sd card to pen drive.

 

#usb #pen-drive #stm32f205rbt6
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Posted on March 10, 2014 at 07:08

Check out STM32F4-Discovery_FW_V1.1.0\Project\FW_upgrade and determine if you can port it back to an F2

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..