cancel
Showing results for 
Search instead for 
Did you mean: 

stm32cube_fw_h7_v1.11.0

sutong
Associate

 

      I can not find     stm32cube_fw_h7_v1.11.0    in the official website, where can download, ask stm32cube_fw_h7_v1.11.0.zip!!!

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
TDK
Super User

https://github.com/STMicroelectronics/STM32CubeH7/archive/refs/tags/v1.11.0.zip

 

Could also get it from installing the package in STM32CubeMX.

If you feel a post has answered your question, please click "Accept as Solution".
STTwo-32
ST Employee

Hello @sutong and welcome to the ST Community :smiling_face_with_smiling_eyes:.

As said @TDK , you can download the stm32cube_fw_h7_v1.11.0 from the github link. But you should not download it as .zip file using the option "download zip" but only using the git commands detailed on the readme file. 

But the easy way will be to download it as a .zip file from our ST website:

Screenshot_2024-03-06-05-18-59-30_40deb401b9ffe8e1df2f1cc5ba480b12.jpg

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.