2026-04-13 5:47 AM - last edited on 2026-04-13 8:26 AM by STackPointer64
Hi
Is there an example using a STM32C5 as a USB host controller connecting a USB HID (mouse/keyboard) as input device?
Solved! Go to Solution.
2026-04-13 6:22 AM
Hello , and Welcome to ST Community!
There is an example in the C5 GitHub repository that you can check out:
Best regards,
2026-04-13 6:22 AM
Hello , and Welcome to ST Community!
There is an example in the C5 GitHub repository that you can check out:
Best regards,
2026-04-13 6:46 AM
Hello @MW
For mouse device please refer to the two examples below:
2026-04-14 1:14 AM
Hello,
If you would like to obtain the examples as standalone projects you can find them through the STM32 Example Library
Best Regards,
Emil