cancel
Showing results for 
Search instead for 
Did you mean: 

Project SBSFU_2_Slots_DualCore for Nucleo-WL55JC1

Alfonzo
Visitor

Hi,

I'm using a Nucleo stm32WL55JC1 board, and i'm trying to run the SBSFU_2_Slots_DualCore example. Used the example selector to start the project. When I tried to compile any of the sub projects they all fail and i have a lot of warnings for include paths that dont exist in my computer. I'm using stm32cubeIDE v2.0.0, i tried using the v 1.11.0 because it said it the release notes that was the version used for STM32Cube_FW_WL_V1.4.0, but the IDE does not accept this package and does not detect it inside the repository folder, even after installing it itself because the examples it shows are from v1.4.0 of the FW package. 

Untitled.png

I also get the error that i can't find the file kms.h that is included in a .c file. When the prebuild.sh runs it runs in the wrong directories, like doing "cd ../../../Middleware.....", in this case there are too many "../" in the path, and this happens a lot in the script.

How can I run this example? What am I missing?

Thanks in advance!

1 REPLY 1
Alfonzo
Visitor

I get the same errors if i try to build the BFU_2_Slots.