Problems with custom bootloader on STM32F4
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-06-01 8:34 AM
Hello,
I have some problems to implement a bootloader in a STM32F4. I searched on internet and I found coherent informations and examples, but I 'm not able to make simple test work.Here my simple code:
bootloader (writed on 0x08000000 address):
&sharpdefine APPLICATION_ADDRESS 0x08008000
typedef void (*pFunction)(void);
pFunction appEntry;uint32_t appStack, test, i;int main(void){
/* Get the application stack pointer (First entry in the application vector table) */
appStack = (uint32_t) *((__IO uint32_t*)APPLICATION_ADDRESS);/* Get the application entry point (Second entry in the application vector table) */
appEntry = (pFunction) *(__IO uint32_t*) (APPLICATION_ADDRESS + 4);/* Reconfigure vector table offset register to match the application location */
SCB->VTOR = APPLICATION_ADDRESS;/* Set the application stack pointer */
__set_MSP(appStack);/* Start the application */
appEntry();while(1);
return 0;
}program (writed on 0x08008000 address):
int main(void){
register uint32_t tl;GPIO_InitTypeDef GPIO_InitStructure;
ErrorStatus HSEStartUpStatus; RCC_DeInit(); // Enable HSE RCC_HSEConfig(RCC_HSE_ON); // Wait till HSE is ready HSEStartUpStatus = RCC_WaitForHSEStartUp(); if(HSEStartUpStatus == SUCCESS){ // HCLK = SYSCLK impostato a 168 tick RCC_HCLKConfig(RCC_SYSCLK_Div1); // PCLK2 = HCLK/2 perch� massimo � 84Mhz RCC_PCLK2Config(RCC_HCLK_Div2); // PCLK1 = HCLK/4 perch� massimo � 42Mhz RCC_PCLK1Config(RCC_HCLK_Div4); // PLLCLK = 168 MHz RCC_PLLConfig(RCC_PLLSource_HSE, 12, 336, 2, 7); // PLLCLK = 144 MHz //RCC_PLLConfig(RCC_PLLSource_HSE, 12, 288, 2, 6); // Enable PLL RCC_PLLCmd(ENABLE); // Wait till PLL is ready while(RCC_GetFlagStatus(RCC_FLAG_PLLRDY) == RESET) { } // Select PLL as system clock source RCC_SYSCLKConfig(RCC_SYSCLKSource_PLLCLK); // Wait till PLL is used as system clock source while(RCC_GetSYSCLKSource() != 0x08){} SystemCoreClockUpdate(); } RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOG, ENABLE); GPIO_InitStructure.GPIO_Pin = GPIO_Pin_4; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP; GPIO_Init(GPIOG, &GPIO_InitStructure);GPIO_SetBits(GPIOG, GPIO_Pin_4);
while(1){
for(tl=0; tl < 0xFFFFFF; tl++); // about 0.6 seconds GPIO_ToggleBits(GPIOG, GPIO_Pin_4); }return 0;
}I write program to 0x08000000 address for test and it works, so I'm sure there is no bugs.When I use bootloader system doesn't work. I try to understand with debugger and I see that instruction appEntry(); has no effect and next command is while(1);
Can anyone tell me where it is wrong?
ThanksRoberto#bootloader #stm-32f407Solved! Go to Solution.
- Labels:
-
Bootloader
-
STM32F4 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-01-15 9:25 AM
If use debugger try to see if the interrupts are enabled. If you have right VTOR value the interrupt might be disabled. I understand that program does not crash i.e. does not go to the Hard_Fault handler...
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-01-16 1:47 AM
SOLVED!
I found that what kept my code from working was that I was trying to launch the application from an ISR. To solve the issue I simply returned from the ISR and launched the application from the main code
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-01-16 2:53 AM
Great! I just implemented my bootloader and was interesting what kind of new issues we can have - different than I came across
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-12-08 9:01 AM
May be you have solved the problem, but...
The question is ( I think): when the application starts at APPLICATION_ADDRESS+4,calls the Reset_Handler that activate the function SystemInit () . This function (as you can read) do
SCB->VTOR = FLASH_BASE | VECT_TAB_OFFSET; (to set vector table address)
but in the application project you have
#define VECT_TAB_OFFSET 0x00 (in system_stm32f4xx.c) and
#define FLASH_BASE 0x08000000U (in my case in stm32f429xx.h).
So now the vector table is at 0x8000000 (this is booloader! not application....)
The boootloader with
SCB->VTOR =APP_ADDRESS;
do a useless thing.
The solution I find? may be inserting in the application code NVIC_SetVectorTable(NVIC_VectTab_FLASH, 0x8000);
or
SCB->VTOR =APP_ADDRESS;
or (I do that) modifyng the file system_stm32f4xx.c
//#define VECT_TAB_OFFSET 0x00
#define VECT_TAB_OFFSET 0x8008000 (or other application APP_ADDRESS).
I hope that a new option in cubeMX (may be there is), ask me the starting address of the application and modify the .ld file and the system_stm32f4xx.c (or the Reset_Handler code).
Ciao!
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-12-08 9:39 AM
You know you can just use the symbol table entry for the vector table that the linker sets to the base of the image as it fixes it for a specific address. No smoke and mirrors, it knows exactly where the image is built to function.
Up vote any posts that you find helpful, it shows what's working..

- « Previous
-
- 1
- 2
- Next »