cancel
Showing results for 
Search instead for 
Did you mean: 

Multiple bulk endpoints, Out Endpoints stalled?

pete
Associate
Posted on February 09, 2014 at 15:59

So I've been working with the Mass storage example in the STM32_USB-FS-Device_Lib_V4.0.0 on the STM32L100RC and I've been happily communicating on a single out and in bulk endpoints.

My application seems to be forcing me into 2 pairs of in and out endpoints, I have added these to the descriptor, sorted the callbacks and the initialization but I cannot receive any data on the added bulk out endpoint (the callback is never called and USBlyzer says endpoint is stalled) in debugging I'm sending back data on the new in endpoint although this seems to be incorrect data which I'm not sure is related?

so I have defined

Endpoint 1 out

Endpoint 2 in

Endpoint 3 out

Endpoint 4 in

and my various bits of code are:

usb_desc

const uint8_t MASS_ConfigDescriptor[MASS_SIZ_CONFIG_DESC] =

{

0x09, /* bLength: Configuration Descriptor size */

0x02, /* bDescriptorType: Configuration */

MASS_SIZ_CONFIG_DESC,

0x00,

0x01, /* bNumInterfaces: 1 interface */

0x01, /* bConfigurationValue: */

/* Configuration value */

0x00, /* iConfiguration: */

/* Index of string descriptor */

/* describing the configuration */

0x80, /* bmAttributes: */

/* Self powered */

0x32, /* MaxPower 100 mA, 500mA == 0xFA */

/******************** Descriptor of Mass Storage interface ********************/

/* 09 */

0x09, /* bLength: Interface Descriptor size */

0x04, /* bDescriptorType: */

/* Interface descriptor type */

0x00, /* bInterfaceNumber: Number of Interface */

0x00, /* bAlternateSetting: Alternate setting */

0x04, /* bNumEndpoints*/

0x00, /* bInterfaceClass: MASS STORAGE Class */

0x00, /* bInterfaceSubClass : SCSI transparent*/

0x00, /* nInterfaceProtocol */

4, /* iInterface: */

/* 18 */

0x07, /*Endpoint descriptor length = 7*/

0x05, /*Endpoint descriptor type */

0x01, /*Endpoint address (out, address 1) */

0x02, /*Bulk endpoint type */

0x40, /*Maximum packet size (64 bytes) */

0x00,

0x00, /*Polling interval in milliseconds */

/* 25 */

0x07, /*Endpoint descriptor length = 7 */

0x05, /*Endpoint descriptor type */

0x82, /*Endpoint address (in, address 2) */

0x02, /*Bulk endpoint type */

0x40, /*Maximum packet size (64 bytes) */

0x00,

0x00, /*Polling interval in milliseconds*/

/*32*/

0x07, /*Endpoint descriptor length = 7*/

0x05, /*Endpoint descriptor type */

0x03, /*Endpoint address (OUT, address 3) */

0x02, /*Bulk endpoint type */

0x40, /*Maximum packet size (64 bytes) */

0x00,

0x00, /*Polling interval in milliseconds */

0x07, /*Endpoint descriptor length = 7 */

0x05, /*Endpoint descriptor type */

0x84, /*Endpoint address (in, address 4) */

0x02, /*Bulk endpoint type */

0x40, /*Maximum packet size (64 bytes) */

0x00,

0x00

//46 bytes

};

usb_conf

#define EP_NUM (5)

#define BTABLE_ADDRESS (0x00)

#define ENDP0_RXADDR (0x18)

#define ENDP0_TXADDR (0x58)

#define ENDP2_TXADDR (0x158)

#define ENDP1_RXADDR (0x118)//I think since each endpoint max siz is set to 64 that all of the buffers can be just 64Bytes further on than each other

#define ENDP3_RXADDR (0x98)

#define ENDP4_TXADDR (0xD8)

/* ISTR events */

/* IMR_MSK */

/* mask defining which events has to be handled */

/* by the device application software */

#define IMR_MSK (CNTR_CTRM | CNTR_WKUPM | CNTR_SUSPM | CNTR_ERRM | CNTR_SOFM \

| CNTR_ESOFM | CNTR_RESETM )

/* CTR service routines */

/* associated to defined endpoints */

#define EP1_IN_Callback NOP_Process

//#define EP2_IN_Callback NOP_Process

#define EP3_IN_Callback NOP_Process

//#define EP4_IN_Callback NOP_Process

#define EP5_IN_Callback NOP_Process

#define EP6_IN_Callback NOP_Process

#define EP7_IN_Callback NOP_Process

//#define EP1_OUT_Callback NOP_Process

#define EP2_OUT_Callback NOP_Process

//#define EP3_OUT_Callback NOP_Process

#define EP4_OUT_Callback NOP_Process

#define EP5_OUT_Callback NOP_Process

#define EP6_OUT_Callback NOP_Process

#define EP7_OUT_Callback NOP_Process

usb_prop

void MASS_Reset()

{

/* Set the device as not configured */

Device_Info.Current_Configuration = 0;

/* Current Feature initialization */

pInformation->Current_Feature = MASS_ConfigDescriptor[7];

SetBTABLE(BTABLE_ADDRESS);

/* Initialize Endpoint 0 */

SetEPType(ENDP0, EP_CONTROL);

SetEPTxStatus(ENDP0, EP_TX_NAK);

SetEPRxAddr(ENDP0, ENDP0_RXADDR);

SetEPRxCount(ENDP0, Device_Property.MaxPacketSize);

SetEPTxAddr(ENDP0, ENDP0_TXADDR);

Clear_Status_Out(ENDP0);

SetEPRxValid(ENDP0);

/* Initialize Endpoint 1 */

SetEPType(ENDP1, EP_BULK);

SetEPRxAddr(ENDP1, ENDP1_RXADDR);

SetEPRxCount(ENDP1, Device_Property.MaxPacketSize);

SetEPRxStatus(ENDP1, EP_RX_VALID);

SetEPTxStatus(ENDP1, EP_TX_DIS);

/* Initialize Endpoint 2 */

SetEPType(ENDP2, EP_BULK);

SetEPTxAddr(ENDP2, ENDP2_TXADDR);

SetEPTxStatus(ENDP2, EP_TX_NAK);

SetEPRxStatus(ENDP2, EP_RX_DIS);

/* Initialize Endpoint 3 */

SetEPType(ENDP3, EP_BULK);

SetEPRxAddr(ENDP3, ENDP3_RXADDR);

SetEPRxCount(ENDP3, Device_Property.MaxPacketSize);

SetEPRxStatus(ENDP3, EP_RX_VALID);

SetEPTxStatus(ENDP3, EP_TX_DIS);

/* Initialize Endpoint 4 */

SetEPType(ENDP4, EP_BULK);

SetEPTxAddr(ENDP4, ENDP4_TXADDR);

SetEPTxStatus(ENDP4, EP_TX_NAK);

SetEPRxStatus(ENDP4, EP_RX_DIS);

SetEPRxCount(ENDP0, Device_Property.MaxPacketSize);

SetEPRxValid(ENDP0);

/* Set the device to response on default address */

SetDeviceAddress(0);

bDeviceState = ATTACHED;

}

I cannot find anything else that I think I should be doing, or any app notes on the subject?....I'm stumped!

If anyone has any suggestions as to what I might be missing then please do chirp in.

#stm32 #usb #stm32l1xx

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0