cancel
Showing results for 
Search instead for 
Did you mean: 

Missing examples in STM32CubeF4 FreeRTOS Package

Posted on April 30, 2015 at 06:03

In UM1722, Developing Applications on STM32Cube with RTOS, DocID025801 Rev 2,

Page 16/26, it says, The STM32CubeF4 FreeRTOS package comes with several applications that use the stack API sets.

I'm sure someone meant to say STOCK, but, where are they, the several applications, that demonstrate things such as Thread Creation, and Queues and Timers and more?

Where are the examples?

#documentation #rtos #examples
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Amel NASRI
ST Employee
Posted on May 19, 2015 at 15:54

Hi Richard,

In the STM32CubeF4 package, some FreeRTOS examples are available under STM32Cube_FW_F4_V1.5.0\Projects\STM324x9I_EVAL\Applications\FreeRTOS.

-Mayla-

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.