cancel
Showing results for 
Search instead for 
Did you mean: 

MCBSTM32C (STM32F107VC) ethernet driver issue

yashdesai93
Associate
Posted on June 24, 2013 at 03:37

Hey,,

I want to implement TCP/IP using no OS on MCBSTM32C (STM32F107VC). The driver ETH_STM32x.c file writen by KEIL uses RTX functions in it's receiving part. 

<i>Therefore i wrote my own function for receiving a frame, everything else is similar to the driver.

</i>

But it is not working. After a lot of checking,<b> i realised it gets stuck at a certain point(second if condition of loop). 

The issue is , the DMA OWN bit in the descriptor is never reset.

 why is this problem arising. </b>

Please Help !!!

my receiving function returns the packet length and it writes the data  from address:packet .

it returns 0 otherwise.

<pre> 

U16 receive_packet( U8 * packet)

{

U32 i,RxLen;

U32 *sp;

i = RxBufIndex;

if (ETH->DMASR &DSR_RS ==0) // check if a packet has been received and buffered

{

return 0;

}

if((Rx_Desc[i].Stat & DMA_RX_OWN) != 0)

{

return 0;

}

 

if( (Rx_Desc[i].Stat & DMA_RX_ES ==0) && ((Rx_Desc[i].Stat & DMA_RX_SEG_MASK) == DMA_RX_SEG_MASK))

{

RxLen = ((Rx_Desc[i].Stat >> 16) & 0x3FFF) - 4;

sp = (U32 *)(Rx_Desc[i].Addr & ~3);

for (RxLen = (RxLen + 3) >> 2; RxLen; RxLen--) 

 {

   *packet++ = *sp++;

 }

}

else

{

RxLen=0;

}

Rx_Desc[i].Stat = DMA_RX_OWN; // Set Own bit of the Rx descriptor Status: gives the buffer back to ETHERNET DMA 

if (++i == NUM_RX_BUF) i = 0;  RxBufIndex = i;

if (ETH->DMASR & INT_RBUIE) 

{ ETH->DMASR   = INT_RBUIE;   // Rx DMA suspended, resume DMA reception. 

ETH->DMARPDR = 0;

}

ETH->DMASR = DSR_NIS | DSR_RS ; // Clear the interrupt pending bits

return(RxLen);

}

</pre>

#mcbstm32c-stm32f107vc-ethernet
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0