cancel
Showing results for 
Search instead for 
Did you mean: 

LWIP Free rtos UDP loopback: what is my mistake??

dieter 123
Associate III
Posted on August 12, 2017 at 08:55

Hi

2 questions here:

1. Why do I need the osDelay(1) before netbuff_delete()? Without it I get a statistical bug/crash.  

2. why do I need lines x1-x3. Without it no second connection is possible.

/*----------------------------------------------------------------------

-------------*/

static void udpecho_thread(void *arg)

{

  err_t err, recv_err;

  LWIP_UNUSED_ARG(arg);

  uint8_t send_buffer[32]={0xff};

  uint16_t len = 0;

  conn = netconn_new(NETCONN_UDP);

  if (conn!= NULL)

  {

    err = netconn_bind(conn, IP_ADDR_ANY, ARTNET_PORT);

    if (err == ERR_OK)

    {

      while (1)

      {

        recv_err = netconn_recv(conn, &buf);

        if (recv_err == ERR_OK)

        {

          addr = netbuf_fromaddr(buf);

          port = netbuf_fromport(buf);

          len = netbuf_len(buf);

          

          if (len < 700)

            netbuf_copy(buf, &MyData, len);

          if (len > 32)

            netbuf_ref ( buf,send_buffer , 32);

          netconn_connect(conn, addr, port);

          

          netconn_send(conn,buf);

          // why do i need this delay??????????

          osDelay(1);

          netbuf_delete(buf);

          //if I uncomment this 3 lines , every thing works fine

          //X1 netconn_delete(conn);

          //X2 conn = netconn_new(NETCONN_UDP);

          //X3 err = netconn_bind(conn, IP_ADDR_ANY, ARTNET_PORT);

      }

      else

      {

        netconn_delete(conn);

      }

     }

  }

 }

}

#lwip #stm32 #netconn #free-rtos
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0