cancel
Showing results for 
Search instead for 
Did you mean: 

Is it required to have HSE clock source for custom bootloader using CAN bus for STM32F446RE

HSing.2
Associate

Hello,

In the application note AN2606, it is mentioned that ST's bootloader for STM32F446RE requires HSE clock if CAN bus is used to upload the hex file.

Now, if I am writing my own custom bootloader to upload the code via CAN, would I still need the HSE clock. Is possible to route HSI clock for the system clock and APB1

Thank you.

Snippet from AN2606

0693W000001sg84QAA.png

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1

You can choose to clock it via any source you want, even ones which are out-of-spec. As long as you're willing to deal with things not work on an occasional unit, and support of that, you can use the HSI

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..