cancel
Showing results for 
Search instead for 
Did you mean: 

Interrupt do not run when resume Swing Thread

Suyog Buradkar
Associate
Posted on October 30, 2017 at 13:23

Hello ST Community,

I have three Threads Running in y code in main function I am declaring 3 Threads and suspend Two of them. My Interrupt Routine calls a function which after words resumes the one Task named 'Swing'. But While this task is running whenever interrupt occurs it does not run at all. 

int main(void)

{

HAL_Init();

SystemClock_Config();

MX_GPIO_Init();

MX_TIM3_Init();

MX_TIM4_Init();

MX_USART1_UART_Init();

MX_USART2_UART_Init();

MX_I2C2_Init();

/* USER CODE BEGIN 2 */

HAL_UART_Receive_IT(&huart2,(uint8_t *)Rx_Data,1);

HAL_TIM_IC_Start_IT(&htim3,TIM_CHANNEL_2);

HAL_TIM_IC_Start_IT(&htim4,TIM_CHANNEL_1);

/* Create the thread(s) */

/* definition and creation of defaultTask */

osThreadDef(defaultTask, StartDefaultTask, osPriorityNormal, 0, 128);

defaultTaskHandle = osThreadCreate(osThread(defaultTask), NULL);

/* USER CODE BEGIN RTOS_THREADS */

/* add threads, ... */

osThreadDef(SwingTask, Swing, osPriorityNormal, 0, 128);

SwingTaskHandle = osThreadCreate(osThread(SwingTask), NULL);

osThreadDef(Task1, Task1, osPriorityNormal, 0, 100);

osThreadCreate(osThread(Task1), NULL);

vTaskSuspend(defaultTaskHandle);

vTaskSuspend(SwingTaskHandle);

vTaskStartScheduler();

/* Start scheduler */

osKernelStart();

/* We should never get here as control is now taken by the scheduler */

/* Infinite loop */

/* USER CODE BEGIN WHILE */

while (1)

{

/* USER CODE END WHILE */

/* USER CODE BEGIN 3 */

}

/* USER CODE END 3 */

}

#multi-tasking #interrups #threads #free-rtos
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0