cancel
Showing results for 
Search instead for 
Did you mean: 

How to sound the audio lineout with STM32H735G-DK

f-fujii
Associate

I'm very beginner of programing and STM.

I'd like to make it sound the audio line out with sine wave from STM32H735G-DK.

I read the document(UM2679) and understood that SAI and I2C4 are connected to the audio.

But I don't know how to use these.

Especially, I couldn't understand how to set volume and start to play.

Attached files are the one I tried and it doesn't work.

I put a button on the screen and set the interaction with function name "startAudio" as it sounds when I push the button.

Please tell me your advice.

I couldn't attach the file Screen1View.cpp.

So I put it down in text below.

 

#include <gui/screen1_screen/Screen1View.hpp>
#include "main.h"
#include <stdio.h>
#include <math.h>

#define SAMPLE_RATE 48000
#define BUFFER_SIZE 1024
#define PI 3.141592

uint8_t audioBuffer[BUFFER_SIZE];

void generateAudioData();


Screen1View::Screen1View()
{

}

void Screen1View::setupScreen()
{
    Screen1ViewBase::setupScreen();
}

void Screen1View::tearDownScreen()
{
    Screen1ViewBase::tearDownScreen();
}

void Screen1View::startAudio()
{
    generateAudioData();
    HAL_SAI_Transmit_DMA(&hsai_BlockA1,(uint8_t*)audioBuffer,BUFFER_SIZE);
}

void generateAudioData(){
    float frequency = 440.0;
    float amplitude = 0.5;
    for(int i = 0; i < BUFFER_SIZE; i++)
    {
        float t = (float)i / SAMPLE_RATE;
        float sine_wave = sin(2 * PI * frequency * t);
        audioBuffer[i] = (uint8_t)((sine_wave * amplitude + 0.5) * 255);
    }
}
1 ACCEPTED SOLUTION

Accepted Solutions
Dor_RH
ST Employee

Hello @f-fujii,

For the STM32H735-DK, the BSP example offers several functionalities:

  • Subdemo 7 and Subdemo 8: These subdemos include a recording feature. The application is designed to use the MB1299 MEMS microphones daughterboard connected to CN20.
  • Subdemo 6: This subdemo includes an AudioPlay feature.

The complete project is available on the STM32CubeH7 page. By following this example, you can successfully output sound through the audio lineout.

I hope my answer has helped you. When your question is answered, please select this topic as solution that answered you, it will help others find that answer faster.

Thanks for your contribution.

Dor_RH

View solution in original post

1 REPLY 1
Dor_RH
ST Employee

Hello @f-fujii,

For the STM32H735-DK, the BSP example offers several functionalities:

  • Subdemo 7 and Subdemo 8: These subdemos include a recording feature. The application is designed to use the MB1299 MEMS microphones daughterboard connected to CN20.
  • Subdemo 6: This subdemo includes an AudioPlay feature.

The complete project is available on the STM32CubeH7 page. By following this example, you can successfully output sound through the audio lineout.

I hope my answer has helped you. When your question is answered, please select this topic as solution that answered you, it will help others find that answer faster.

Thanks for your contribution.

Dor_RH

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.