cancel
Showing results for 
Search instead for 
Did you mean: 

Getting started with analog, STM32F769I-DISCO. undefined reference to wm8994_drv

HTiwa.3
Associate

I am trying this example on my STM32F769I-DISCO. I followed the given tutorial for adding the dependecy. wm8994 is in ../Components/wm8994/wm8994.h.

But when building the code I am getting

../stm32disco/test2_audioread/Debug/../Core/Src/main.c:1263: undefined reference to `wm8994_drv'

Tutorial link : https://wiki.st.com/stm32mcu/wiki/STM32StepByStep:Getting_started_with_analog

Edit: When I looked the header file it is defined as extern. So it may be a problem how it can be resolved.

/* Audio driver structure */

extern AUDIO_DrvTypeDef   wm8994_drv;

#endif /* __WM8994_H */

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Imen.D
ST Employee

Hello @HTiwa.3​ ,

Make sure your project contains the include libraries pathing set up correctly with the dependencies.

So, you need to set up correctly the "Include Paths" for the project.

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen