cancel
Showing results for 
Search instead for 
Did you mean: 

emWin project examples for STM32H745I-DISCO evaluation board

MBada
Associate

In order to evaluate emWin graphics library, I'm using the evaluation board STM32H745I-DISCO and I'm trying the example project "STemWin_HelloWorld".

When I call GUI_DispStringAt ("hello",0,0) I see that the string is not displayed from X = 0 position, but from an X offset of some pixels. Also the "STemWin_SampleDemo" example project have all the windows that start from an offset from the left of display. What could be the problem?

Thanking in advance,

Massimo Badanai

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0