cancel
Showing results for 
Search instead for 
Did you mean: 

datapro 1 pack is corrupt

RB4
Associate

 

Can someone please provide a working download file for "STM32Cube function pack for STEVAL-PROTEUS1 sensor datalog and file transfer over BLE and USB"?

The ZIP-File Version is corrupt.

It cannot be extracted neither on Windows, Linux or Mac.

Thank you.

@

1 REPLY 1
Peter BENSCH
ST Employee

I have just downloaded and checked FP-SNS-DATAPRO1 again - the archive is consistent and unpacking works without any problems.

If none of the checksums of the ZIP (version 1.1.0) match, you should download the archive again, possibly on a different computer, as sometimes there are problems in university networks or behind proxies:

  • SHA-1: 451BBD700FC0E84C38DF14CEAFFCD54FAD6755EE
  • SHA-256: 9A7146747F38DFF837CDD3C3AA34F0AE0BDE460FA518E7BAD130C3D3B9BD6335

Hope that helps?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.