cancel
Showing results for 
Search instead for 
Did you mean: 

Bootloader Problem

andrewkelly9
Associate II
Posted on February 12, 2010 at 17:23

Bootloader Problem

#bootloader
This discussion is locked. Please start a new topic to ask your question.
13 REPLIES 13
Posted on May 17, 2011 at 13:40

Check the MAP/HEX files to confirm the base address of the application code.

It is important that the low order address bit of any code you jump to is 1, the STM32 can only execute THUMB code.

I export the address of the vectors in the application start up code, then use that to set the address. So provided you don't violate any alignment rules, the application is agnostic to the location it is loaded.

In the startup.s file

               EXPORT  __Vectors

In the application.c file

extern void * __Vectors;

NVIC_SetVectorTable((u32)(&__Vectors), 0x0); // Smart Base Location

Some assembler to enter the system boot loader looks like this, change the address to reflect the base address of you application.

Reboot_Loader    PROC

                EXPORT    Reboot_Loader

                LDR        R0, =0x1FFFF000

                LDR        SP,[R0, #0]

                LDR        R0,[R0, #4]

                BX        R0

                ENDP

-Clive
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
andrewkelly9
Associate II
Posted on May 17, 2011 at 13:40

Could the odd boundary be my problem. I am locating code at 0x8004000 and attempting to run it.(on Even boundary). Don't know anything about thumb alignment. It is the entire binary that I am copying to this location.

My Code code was:

void app_start(void)

{

    void (*app)();

    irq_disable();

    runapp=(void(*)())(0x8004000);

    app();

}

Replaced with the code you gave and still the same. I think IRQs are a distraction, it should still start?

.arm

.text

global       start_application

start_application:

                ldr        R0, =0x1FFFF000

                ldr        SP,[R0, #0]

                ldr        R0,[R0, #4]

                BX        R0

Thanks

Posted on May 17, 2011 at 13:40

The code assumes you have the Stack Pointer and Start Address as the first two words of the image.

If the first half-word is an instruction, you would need to jump to 0x8004001, as you are running Thumb code, not ARM code.

-Clive
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
andrewkelly9
Associate II
Posted on May 17, 2011 at 13:40

Sorry that address was

start_app:

                ldr        R0, =0x8004000

                ldr        SP,[R0, #0]

                ldr        R0,[R0, #4]

                BX        R0

andrewkelly9
Associate II
Posted on May 17, 2011 at 13:40

No Luck. The start of Rom where it is jumping to starts with the IRQ table

so I presume that can start at location:0x8004000

I have no memory protection stuff turned on.

Does anyone know of any sample code that jumps to another location in Rom?

(written in C):

__attribute__ ((section(''.isr_vector'')))

void (* const g_pfnVectors[])(void) =

{

    (void (*)(void))((unsigned long)stack + sizeof(stack)),

                                            // The initial stack pointer

    ResetISR,                               // The reset handler

    NmiSR,                                  // The NMI handler

    FaultISR,                               // The hard fault handler

etc.

Posted on May 17, 2011 at 13:40

You're going to need to examine the code/data generated by the compiler/linker. Unless the correct addresses and linkage is occurring this isn't going to work.

Try using a

JTAG

debugger and single stepping the critical code to ensure it is doing what you expect.

-Clive

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
andrewkelly9
Associate II
Posted on May 17, 2011 at 13:40

I have looked at AN2557 and there doesn't appear to be much in it.

I am using GCC, so the function

NVIC_SetVectorTable(NVIC_VectTab_FLASH, 0x4000);

doesn't appear to be available to me.

Looking at the map file though, the vectors are located at 0x8004000

The definition is as follows:

__attribute__ ((section(''.isr_vector'')))

void (* const gpVectors[])(void) =

{

    (void (*)(void))((unsigned long)stack + sizeof(stack)),

and mapfile gives :

.isr_vector    0x08004000      0x130 bin/startup.o

                0x08004000                gpVectors

 

 So happy there.

 I thought that maybe it was an alignment issue.

 I copy the binary to 0x8004000

 but maybe I should be runninfg the application from

 0x8004001

 (Bt the way, application runs fine without bootloader)

My code to run application is:

#define APP_ORIGIN 0x8004000

void app_start(void)

{

    void (*runapp)();

    irq_disable();

    runapp=(void(*)())APP_ORIGIN;

    runapp();

}

have also tried

runapp=(void(*)())(APP_ORIGIN+1);

andrewkelly9
Associate II
Posted on May 17, 2011 at 13:40

I will study the sample app, this is useful.

I notice they run

app_address+4

when running the application, tried it quickly, bur I still crash.

I will left you know if I get success from the app note.

Thanks

Posted on May 17, 2011 at 13:40

Ok, you don't need to change the load location to 0x8004001, the low order bit simply flags to the program counter that the code in question is THUMB code. All code on the STM32 (Cortex-M3) must be THUMB, it cannot execute 32-bit ARM code.

Also remember that the first vector entry is the address of the stack top in RAM, the second entry is the reset vector. It is the address of the reset vector, not executable code.

The assembler code to execute from a vector table would be

                LDR        R0, =0x08004000

                LDR        SP,[R0, #0]

                LDR        R0,[R0, #4]

                BX        R0

If NVIC_SetVectorTable() is not available you will need to reprogram the NVIC directly to point the hardware to the vector table.

-Clive

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..