Skip to main content
Kk1
Associate
Jun 8, 2021 1:24 PM UTC
Question

azure RTOS connectivity with Nucleo-h745zi-q?

I am working on a Nucleo-h745zi-q controller. I want to connect the stm32h7 board with Microsoft azure. I installed the package on stm32ide x-cube-azrtos-h7. But I did not know how I can connect to azure. What is the procedure for using this Rtos connectivity?

This topic has been closed for replies.

6 replies

ST Technical Moderator
Jun 8, 2021 3:30 PM UTC

Hello @Kk​ and welcome to the Community :)

I added the right topics to your question in order to increase its chance to be reviewed by our experts, and I would also suggest you adding more details to your post in order to help you. 

Maybe these links are useful for you:

Thanks

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
Cartu38 OpenDev
Graduate II
Jun 8, 2021 8:04 PM UTC

@Kk​ sorry but what is question / issue here ? Please be a little be more explicit if expecting some help ...

Kk1
Kk1Author
Associate
Jun 9, 2021 7:18 AM UTC

I am working on stm32h745zit6 controller. I want to connect the stm32h7 board with microsoft azure. I installed the package on stm32ide x-cube-azrtos-h7.But i did not know how i can connect to cloud azure. Means i have to do login to microsoft azure? What is the procedure for accessing the microsoft azure. Can you help me?

Guillaume K
ST Employee
Jun 9, 2021 11:38 AM UTC

Hello,

The x-cube-azrtos-h7 package provides Azure RTOS support and NetX Duo network stack support on STM32H7. There is no specific support for Azure Cloud in this package. As you have Azure RTOS and network support on STM32H7 I guess you can just use Microsoft's examples and support for Azure IoT Cloud on their web site and github.

Guillaume K
ST Employee
Jun 9, 2021 11:46 AM UTC

for MS Azure Cloud SDKs see https://github.com/Azure/azure-iot-sdks , especially Azure IoT SDK for embedded C

  • Azure IoT SDK for Embedded C is an alternative for constrained devices which enables the BYO (bring your own) network approach: IoT developers have the freedom of choice to bring MQTT client, TLS and Socket of their choice to create a device solution
  • Azure IoT SDK for C written in ANSI C (C99) for portability and broad platform compatibility. There are two device client libraries for C, the low-level iothub_ll_client and the iothub_client (threaded).

Guillaume K
ST Employee
Jun 9, 2021 11:43 AM UTC

if you are using stm32h745zit6 , I don't see it in x-cube-azrtos-h7 package. So what kind of board are you using ? what network interface does it have ? ethernet ?

To be able to connect to Azure Cloud you need Azure RTOS and TCP/IP stack (NetX). If the network interface is not the same as the one supported in x-cube-AZRTOS-h7 you will have to implement in NetX Duo the network driver for it.