2024-12-19 4:56 PM
Hello,
I recently bought the newly released development kit STM32N6570-DK that includes a touch screen and a MIPI camera manufactured by ST. It comes preprogrammed with some nifty demos, including the AI demo which should show off the AI capabilities with a stream from the included camera. When I load the AI demo the screen freezes up, and I can see the backlight to the screen turn off.
Additionally I noticed there are some level shifters (TR1 on the camera module) on the PCB for the camera that either carry a clock or data line for MIPI. When I activate the demo the 3.3V line starts toggling at about 160MHz for about 2ms, and then stays low after that.
For reference, I am powering the dev kit off of a USB 3.0 port on my laptop.
Could you help me identify if this is a camera module, dev kit, power, or cable issue?
Thanks,
-Alex
Solved! Go to Solution.
2025-12-15 9:21 AM
Thanks. That worked perfectly.
I was worried that I had damaged something. For anyone else experiencing this, look at L03. When connected to a USB-A on my laptop, it came up yellow and changed to red when I started the AI demo. With power from a USB-C port on my laptop, it came up green and stayed green when the demo started.