2024-11-22 4:11 PM
Can somebody tell me whether I am, or not, powering this STM32H725RG in the right way?
As far as I know, after reading several times the specs, the 68 pin package doesn't have LDO (SMPS only).
I've built my first board this way and the MCU got burnt.
Thanks.
2026-03-09 3:53 PM
KiCAD isn't hiding duplicate VDD or VCAP pins. I'm not buying that VSS pins are treated differently.
2026-03-09 4:27 PM
In this symbol, it is.
Anyway, unconnected pins it's not the cause. I can assure that. Everything is connected as it has to.