cancel
Showing results for 
Search instead for 
Did you mean: 

[Nucleo-N657X0-Q ]How to use swv printf in Keil arm mdk 5.39

bioak
Associate

I would like to use SWV for debugging on the Nucleo-N657X0-Q board.

I first enabled SWV debugging and also change the CPU clock to 400 MHz.

 

image.png

 

bioak_0-1750155820298.png

 

Then, I added some code to main.c (as reference here ).

bioak_3-1750157556553.png

bioak_1-1750156771078.png

At the same time, I also set the core clock to 50 MHz in the TRACE configuration of Keil.

bioak_2-1750156875457.png

But i can't see any string in Debug Viewer.

Does anyone know what else I should check?

 

Thank's 

0 REPLIES 0