cancel
Showing results for 
Search instead for 
Did you mean: 

Thermal resistance Rja and Rca of ST25R3916-AQWT

MK.12
Associate II

Hello,

I would like to receive information on the thermal characteristics of ST25R3916-AQWT.

Rja and Rca.

Let me know your input!

Cheers

Madhu

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions

Hello Madhu,

Rtheta_jc is specific to the device (more in detail it is specific to the used package).

This is why we can very precisely can name this number.

Rthetha_ja is specific to the device / package, PCB (size, amount of copper, number of layers, ...) and housing / airflow. This means, this number (Rthetha_ja) is specific to the application itself and we cannot do a general statement here.

This is why we did this application note, showing how to setup the thermal model and measure / calculate the thermal resistance of each node (e.g. ja an ca on bottom and top).

BR Travis

View solution in original post

3 REPLIES 3
Ulysses HERNIOSUS
ST Employee

Hi Madhu,

did you find and check AN5584: ST25R39xx NFC reader thermal design?

Best Regards, Ulysses

MK.12
Associate II

Hello Ulysses,

I did check the document. I was able to find Rtheta_jc as 16.95C. I dont think Rthetha_ja is not listed if I am right. So is it possible to get the correct value for Rthetha_ja?

Cheers

Madhu

Hello Madhu,

Rtheta_jc is specific to the device (more in detail it is specific to the used package).

This is why we can very precisely can name this number.

Rthetha_ja is specific to the device / package, PCB (size, amount of copper, number of layers, ...) and housing / airflow. This means, this number (Rthetha_ja) is specific to the application itself and we cannot do a general statement here.

This is why we did this application note, showing how to setup the thermal model and measure / calculate the thermal resistance of each node (e.g. ja an ca on bottom and top).

BR Travis