cancel
Showing results for 
Search instead for 
Did you mean: 

That is 1 Ohm between AC0 and AC1 in X-NUCLEO-NFC04A1 ?

John_zhang
Associate II

Antenna is about 5 Ohm and 4.5uH, why is 1Ohm?

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Denis ROMAN
Associate III

​Hello Zhang,

For ST25DV64k, Cs is also 28.5pF. You thus just need to design/use an antenna which inductance around 4.5uH, there is not need for additional resistor.

Have a nice day

Denis

View solution in original post

6 REPLIES 6
AvaTar
Lead

Probably to disconnect the antenna easily with removing the resistor.

Denis ROMAN
Associate III

​Hello Zhang,

I am really sorry but I don't understand your point.

Denis

I hope to design R and L value of the st25dv64 external antenna, not internal PCB antenna by tool. In the AN2972 document, “2.3 Basic equations “ , I don’t know Rs and Cs. So I could not designed antenna of st25dv64. In the other document about M24LR64, Cs is 28.5pF, Rs is 5Ohm. By those parameters, I would calculate R and L of M24LR64 antenna, Ra is 5Ohm , L is 4.5uH. I hope to test real resistor between AC0 and AC1of St25dv64 with the X-NUCLEO-NFC04A1. The test resistor value is1Ohm, not 5Ohm or2.5Ohm. Thanks!

Hi,

Thanks for your reply. Which resistor to remove?

Thanks!

BR

zhang

Denis ROMAN
Associate III

​Hello Zhang,

For ST25DV64k, Cs is also 28.5pF. You thus just need to design/use an antenna which inductance around 4.5uH, there is not need for additional resistor.

Have a nice day

Denis

Hello Denis

Thanks.It is important for me.

Have a nice day!

BR,

zhang​