cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeExpansion_NFC4 set RF password with I2C

Mickaël Bucher
Associate II

Hi,

I use a ST25DV04K with STM32CubeExpansion_NFC4_V2.0.2.

 is it possible to set a RF password with an I2C function ?

if yes, Could you give me some examples ?

Best regards

Mickaël

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
JL. Lebon
ST Employee

Hello Mickaël,

It is not possible to write or read RF passwords from the I2C interface.

It is also not possible to write or read I2C password from RF interface.

The passwords and security sessions for RF and I2C are completely independent and isolated for security reasons.

Best regards.

View solution in original post

1 REPLY 1
JL. Lebon
ST Employee

Hello Mickaël,

It is not possible to write or read RF passwords from the I2C interface.

It is also not possible to write or read I2C password from RF interface.

The passwords and security sessions for RF and I2C are completely independent and isolated for security reasons.

Best regards.