cancel
Showing results for 
Search instead for 
Did you mean: 

ST25RU3993-HPEV with NUCLEO-L476RG

PRena.1
Associate II

Hello,

I successfully succeed to control my ST25RU3993-HPEV with my external MCU.

I can detects all my tags just in a area of 10 cm, but my External PA is activated. I don't know what parameters i have to change to allows at my system to detect my tags in a area of 10 m ?

I also see a consumption of 0.7 A so i think that the PA is running good.

And i use the default parameter in the FW wich is on this link 

Someone can help me pls ? 

 

Thanks you !

 

Paul :) 

 

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Marcel Rossignol
ST Employee

Hello Paul,

which tags and which reader antenna are you using?

Best regards,

Marcel