cancel
Showing results for 
Search instead for 
Did you mean: 

ST25RU3993-HPEV PIE encoding pulse width (PW)

MYoun.4
Associate II

Hi :)

I know ST25RU3993 use PIE encoding when it transmits data.

In EPC Gen-2 protocol, PW (pulse width, in attached image) used in PIE has a value:

MAX(0.265Tari, 2 μs)<=PW<=0.525Tari

I want to know what range of PW ST25RU3993-HPEV can use.

Thank you.

0693W00000DmUHZQA3.jpg

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Bart Herse
Senior II

Hi MYoun.4,

let me refer to the datasheet of ST25RU3993.

In Table 12 on page 49, explaining the purpose of the TX options register, it is shown that the TARI can be set to 6.25µs, 12.5µs and 25µs.

The PIE symbol for a logic one can be changed in the same register.

Using the bits TXOne[1:0] the length of a PIE-"1" can be changed.

There is no way to change PW directly, but PW will be always half of TARI value.

Cheers,

B

View solution in original post

1 REPLY 1
Bart Herse
Senior II

Hi MYoun.4,

let me refer to the datasheet of ST25RU3993.

In Table 12 on page 49, explaining the purpose of the TX options register, it is shown that the TARI can be set to 6.25µs, 12.5µs and 25µs.

The PIE symbol for a logic one can be changed in the same register.

Using the bits TXOne[1:0] the length of a PIE-"1" can be changed.

There is no way to change PW directly, but PW will be always half of TARI value.

Cheers,

B