cancel
Showing results for 
Search instead for 
Did you mean: 

ST25R3917 as direct replacement in a ST25R3916 project

LHing.1
Associate

Can the ST25R3917 be used as direct replacement in a ST25R3916 project based on X-NUCLEO-NFC06A1, or do I need to change anything in the code?

I am aware that some hardware features aren't available.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Ulysses HERNIOSUS
ST Employee

Hi LHing.1,

yes it can be used as a direct replacement. If you have code running on ST25R3916 which is not using any features not available on the 3917 then it will run out of the box on ST25R3917.

Best Regards, Ulysses

View solution in original post

3 REPLIES 3
Brian TIDAL
ST Employee

Hi,

is it X-NUCLEO-NFC05A1 (ST25R3911B based) or X-NUCLEO-NFC06A1 (ST25R3916 based)?

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
LHing.1
Associate

It is X-NUCLEO-NFC06A1 based, I'll fix the typo.

Ulysses HERNIOSUS
ST Employee

Hi LHing.1,

yes it can be used as a direct replacement. If you have code running on ST25R3916 which is not using any features not available on the 3917 then it will run out of the box on ST25R3917.

Best Regards, Ulysses