2024-04-15 10:28 PM
Hi,
is it possible to use the ST25R3916B with an resisitve divider (instead of the capacitive divider) at the RF Inputs to limit the input voltage to a safe value.
In case this is possible, is an additional DC-Block needed?
I am driving a purely resistive load with the RF Outputs.
Thank you very much.
Moritz
Solved! Go to Solution.
2024-06-12 01:57 AM
Hi,
The chip is biasing the input signal (sinus) coming from the antenna using AGD voltage.
It means that the sinus is DC biased by ~1.5V. Therefore the Antenna needs to be DC de-coupled from the antenna.
All the internal filters are designed in a way to operate with this proposed capacitiv voltage divider.
A resisitve voltage divider is not recommended and operation is not guaranteed.
BR Travis
2024-06-12 01:57 AM
Hi,
The chip is biasing the input signal (sinus) coming from the antenna using AGD voltage.
It means that the sinus is DC biased by ~1.5V. Therefore the Antenna needs to be DC de-coupled from the antenna.
All the internal filters are designed in a way to operate with this proposed capacitiv voltage divider.
A resisitve voltage divider is not recommended and operation is not guaranteed.
BR Travis
2024-06-12 05:24 AM
Hi Travis,
thank you very much.
Kind regards
Moritz