Skip to main content
Associate
June 7, 2024
Solved

ST25R3911B-DISCO communication with Labview

  • June 7, 2024
  • 1 reply
  • 1744 views

Hi,

I've purchased the ST25R3911B-DISCO and it's working fine with ST25PC-NFC.exe.

I would like to communicate via uart with ST25R3911B-DISCO in order to implement the tag reading in Labview. There is any document that explain how to create packets to communicate via uart? Or there is any mode of using ST25PC-NFC.exe without GUI and implement the communication via command window?

 

Thank for the support

This topic has been closed for replies.
Best answer by Ulysses HERNIOSUS

Hi,

the Disco software is more focused on data exchange and not so much on identifying and issuing the commands necessary to perform R/W operations on the different memory tags.

Maybe you are then really better off with the ST25 SDK.

Regards, Ulysses

1 reply

Ulysses HERNIOSUS
ST Technical Moderator
June 10, 2024

Hello Riccardo96,

you could either use the ST25 SDK which can interface with the ST25R3911B-DISCO board or use the ST25R3911B-DISCO GUI which comes with a DLL and demo projects showcasing NFC communication from C++, C# and Python.

Ulysses

Associate
June 10, 2024

Hello Ulysses,

First of all thanks for the quick answer.

The ST25 SDK you are mentioning is this one: STSW-ST25SDK001 - Software Development Kit for ST25 Tags and Dynamic Tags - STMicroelectronics ?

Also, where can i download the ST25R3911B-DISCO GUI? This i think will be the best solution because i can easly use python with Labview, but i don't see where to find these demo. I think i've read somewhere that this demo will be located in the document folder on my user path but i don't see anything.

Riccardo

Ulysses HERNIOSUS
ST Technical Moderator
June 10, 2024

Hi Riccardo,

 

ad 1: correct

ad 2: The demo is part of STSW-ST25R001. In its installation folder you will find a shortcut to Dll3911_Demos.sln somewhere in your user folder.

 

Ulysses