cancel
Showing results for 
Search instead for 
Did you mean: 

Problem using listen mode on the st25r3916b

JBark.3
Associate II

I am trying to use the st25r3916b in listen mode to act as an NFCA card.

After successful calls to rfalNfcInitialize() and rfalListenStart(RFAL_LM_MASK_NFCA, ...) I am entering into a loop and calling rfalWorker(). In the same loop I call rfalListenGetState to try and see if any data comes back from the reader, which never does.

After debugging this some, I can see that inside rfalRunListenModeWorker (called from rfalWorker) always goes through the following state change:

RFAL_LM_STATE_POWER_OFF ->

RFAL_LM_STATE_IDLE ->

RFAL_LM_STATE_POWER_OFF

This seems to be happening because ST25R3916_IRQ_MASK_EOF is set on the st25r3916b's register. This feels strange because ST25R3916_IRQ_MASK_EON is also set, which is required for it to leave the idle state in the first place.

I feel like the chip is not configured properly, but I have no idea why.

Notes about setup:

X-NUCLEO-NFC08A1 dev board connected to NUCEL F401RE dev board.

I have successfully tested the setup in polling mode and can read cards no problem.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Ulysses HERNIOSUS
ST Employee

Hi,

what is the counter part you are using? A phone? Better to start off with another st25r39... reader and executing field-on, Send a request, etc. driven by a GUI.

Reason is that phones are doing wake-up and very fast polling and depending on the timing of your port you may miss to go into the right states fast enough.

Having I_eon and I_eof together is often an effect of a phone performing short (few us) pulses to detect a detuning in its tank (wake-up aka LPCD).

As reference please also get NUCLEO-L476 and run the stop demos from ST25 embedded NFC lib which contains a ready working card emulation demo (pairing).

Best Regards, Ulysses

View solution in original post

4 REPLIES 4
Ulysses HERNIOSUS
ST Employee

Hi,

what is the counter part you are using? A phone? Better to start off with another st25r39... reader and executing field-on, Send a request, etc. driven by a GUI.

Reason is that phones are doing wake-up and very fast polling and depending on the timing of your port you may miss to go into the right states fast enough.

Having I_eon and I_eof together is often an effect of a phone performing short (few us) pulses to detect a detuning in its tank (wake-up aka LPCD).

As reference please also get NUCLEO-L476 and run the stop demos from ST25 embedded NFC lib which contains a ready working card emulation demo (pairing).

Best Regards, Ulysses

Thanks for the info.

I had been suspicious of the timing so I am not surprised to hear this suggestion. I noticed that my app has more success when I turn off usart logging so I am guessing that my paranoid debugging logs might be causing some issues, this will make this quite hard to investigate if I cannot use logs or breakpoints. I wonder if I need to maintain an in memory log and then dump to usart at a less time sensitive moment.

JBark.3
Associate II

@Ulysses HERNIOSUS_O​ this is all working now, mostly!

Everything is working and my emulated card is picked up by the reader device with all the right data.

I am now seeing an issue where my firmware locks up after an amount of time. It's sometimes after a couple of scans, sometimes right away.

Debugging this I can see that my code gets stuck here st25r3916CheckForReceivedInterrupts, it's stuck in here while( platformGpioIsHigh( ST25R_INT_PORT, ST25R_INT_PIN ) ) because the interrupt pin never goes low.

I am not sure how to debug this further since this is the st25r3916b keeping the pin high.

Hi,

the st25r3916CheckForReceivedInterrupts() is issuing calls to read the interrupt status register of the st25r3916. Is this read correctly executed? What is the register content it is reading?

Regards, Ulysses