cancel
Showing results for 
Search instead for 
Did you mean: 

NFC05A1

MatteoBandini74
Associate II

I'm using XCube for develope. Can I use NFC6 for this board?

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Brian TIDAL
ST Employee

Hi,

X-CUBE-NFC6 is designed for ST25R3916 not for ST25R3911B.

For X-NUCLEO-NFC05A1 (ST25R3911B), X-CUBE-NFC5 has to be used. X-CUBE-NFC5 is a standalone package. See Solved: How to create a project with X CUBE NFC06 - STMicroelectronics Community on how to import the X-CUBE-NFC5 package into a STM32CubeMX generated project.

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Brian TIDAL
ST Employee

Hi,

X-CUBE-NFC6 is designed for ST25R3916 not for ST25R3911B.

For X-NUCLEO-NFC05A1 (ST25R3911B), X-CUBE-NFC5 has to be used. X-CUBE-NFC5 is a standalone package. See Solved: How to create a project with X CUBE NFC06 - STMicroelectronics Community on how to import the X-CUBE-NFC5 package into a STM32CubeMX generated project.

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.