2020-02-17 7:24 AM
Hi,
Kindly help me sharing the link or source of ST25RU3993 's library files for BUS, PROTOCOL, DISPATCHER layer. (Document UM2618 does not says about these layers, it is said as NOT EXPOSED LAYER).
Thanks
Solved! Go to Solution.
2020-03-08 11:44 PM
hi, SDK source code package includes the complete source code of the STM32L4 based FW the middleware and demo samples for host side usage on windows and linux. This also includes the mentioned NOT EXPOSED LAYERs. NOT EXPOSED here means that these modules do not have exposed API and are used implicit when using the API.
The SDK source code package could be found on st.com
BR
Nick
2020-03-08 11:44 PM
hi, SDK source code package includes the complete source code of the STM32L4 based FW the middleware and demo samples for host side usage on windows and linux. This also includes the mentioned NOT EXPOSED LAYERs. NOT EXPOSED here means that these modules do not have exposed API and are used implicit when using the API.
The SDK source code package could be found on st.com
BR
Nick
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.