2025-03-10 7:37 AM
Hello all,
I discovered that selecting in STM32CubeIDE under Pinout & Configuration/Middleware and Software Packs/ X-CUBE-NFC4 the source folder Middleware/ST/lib_nfc is added to the project source tree, containing the source files for the lib_nfc library.
However, while the support fot NFC Type 5 appears complete, the support for Type 4 is not.
Are there plans to complete the support?
Thanks,
Adriano
Solved! Go to Solution.
2025-04-03 8:11 AM
Hi Adriano,
The X-CUBE-NFC4 software expansion is dedicated to ST25DV Type 5 dynamic tag. As this is a Type 5 Tag, the lib_nfc provides type 5 support.
Can you elaborate on your need for T4T support: is this for a reader or for a tag?
NFC readers such as ST25R95, ST25R3911B, ST25R3916/16B, ST25R200 or ST25R300 supports communication with various types of tag including T4T. The ST25 Embedded library provides the various middleware for reading/writing NDEF messages from/to T2T, T3T, T4T or T5T tags.
Rgds
BT
2025-04-03 8:11 AM
Hi Adriano,
The X-CUBE-NFC4 software expansion is dedicated to ST25DV Type 5 dynamic tag. As this is a Type 5 Tag, the lib_nfc provides type 5 support.
Can you elaborate on your need for T4T support: is this for a reader or for a tag?
NFC readers such as ST25R95, ST25R3911B, ST25R3916/16B, ST25R200 or ST25R300 supports communication with various types of tag including T4T. The ST25 Embedded library provides the various middleware for reading/writing NDEF messages from/to T2T, T3T, T4T or T5T tags.
Rgds
BT