Skip to main content
JDirk.1
Associate III
November 7, 2020
Solved

Information about the possibility to upgrade Firmware on STM32

  • November 7, 2020
  • 1 reply
  • 636 views

I have heard the ST25DV can be used to upgrade the Firmware of any STM32 Microcontroller. I would like to understand how this is done. Also how the PINs needs to be connected to the STM32. Or is the code transfered via I2C? If so, how does the STM32 know where to place the code? I need general information about this topic. Maybe someone could let me know where to find information (best practices etc.)

many thanks in advance

Baris Yilmaz is talking about, see 1:12 (i cant understand the name, he is talking too fast ...)

https://www.youtube.com/watch?v=h0895kgTPO0

This topic has been closed for replies.
Best answer by Ulysses HERNIOSUS

Hi,

I think @Baris YILMAZ​ is talking about the fast transfer mode (mailbox) of ST25DV together with SBSFU (acronyms are always hard to understand) of the STM32. I guess you can checkout details in the X-CUBE-SBSFU package.

Regards, Ulysses

1 reply

Ulysses HERNIOSUS
ST Technical Moderator
November 8, 2020

Hi,

I think @Baris YILMAZ​ is talking about the fast transfer mode (mailbox) of ST25DV together with SBSFU (acronyms are always hard to understand) of the STM32. I guess you can checkout details in the X-CUBE-SBSFU package.

Regards, Ulysses