cancel
Showing results for 
Search instead for 
Did you mean: 

How to set up IRQ pin if i just want to read the RSSI of ST25RU3993

XChen.1
Associate II

I posted a tread last week but it soon got buried....

So I wasn't able to get any output when probe or read from MISO using Arduino due.

and @Bart Herse​  asked me in the post have i connected my IRQ pin.

After reading the data sheet I am still not sure what to do with my IRQ signal coming out of ST25. Currently when I probe the IRQ output stays HIGH...I am using the EVAL ST25RU3993

here is my Arduino code, I just want to read RSSI information under default set up.

#include <SPI.h>
////////////////////////////////////////////
//set up pins for arudino due
//MOSI:ICSP-4
//MISO:ICSP-1
//SCK:ICSP-3
//NCS:52
//EN:2
//IRQ:22
///////////////////////////////////////////////
 
// Set up chip-select pin as NCS and enable pin as EN
const int NCS = 52;
const int EN = 2;
const int IRQ =7;
 
//SPI setting
SPISettings settingsA(100000, MSBFIRST, SPI_MODE0);
 
void setup() {
 
  pinMode (NCS, OUTPUT);
  pinMode(EN, OUTPUT);
  pinMode(IRQ, INPUT);
  digitalWrite(EN, HIGH);//set enable to high
  Serial.begin(9600);
 
  SPI.begin();
  SPI.beginTransaction(settingsA); //I wrote to the following 2 main control registers, register description is at the data sheet
 
//  digitalWrite (NCS, LOW);
//  SPI.transfer(0b00000000); // write and register addressL: Device staus register
//  SPI.transfer(0b00000001); // value for this register: Turn RF-On
//  digitalWrite (NCS, HIGH);
 
//  digitalWrite (NCS, LOW);
//  SPI.transfer(0b00000001); // write and register addressL: Protocal Selection Register
//  SPI.transfer(0b00000000); // value for this register: Choose EPC Gen2
//  digitalWrite (NCS, HIGH);
  Serial.print("written");
 
   SPI.endTransaction();
}
 
 
int8_t O;
void loop() {
  //
  for (int i = 0; i <= 25500; i++) {
 
      SPI.beginTransaction(settingsA); //read from my RSSI_Display register
    digitalWrite (NCS, LOW);
 
 O =   SPI.transfer16(0b0110101100000000);
 //   SPI.transfer(0b0100000);
 
    digitalWrite (NCS, HIGH);
     SPI.endTransaction();
  //   delay(50);
 
  }
  Serial.print(O);
}

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Bart Herse
Senior II

The IRQ pin notifies the MCU when events such as TX done, etc. have happened. When IRQ pin goes high the FW enters the IRS and checks the registers 0x37 and 0x38 to read out the interrupt source. Reading from these two registers will reset the IRQ pin.

Cheers,

B

View solution in original post

1 REPLY 1
Bart Herse
Senior II

The IRQ pin notifies the MCU when events such as TX done, etc. have happened. When IRQ pin goes high the FW enters the IRS and checks the registers 0x37 and 0x38 to read out the interrupt source. Reading from these two registers will reset the IRQ pin.

Cheers,

B