Skip to main content
Simon R.
Associate
August 28, 2018
Solved

Having difficulties loading/reading FIFO of ST253911B

  • August 28, 2018
  • 2 replies
  • 1140 views

Edit: I solved the problem, it was my own fault! The Operation Control Register's bit 7 was set to 0 when it should have been set to 0. Thanks!

--------------------------------------------------------------

Hello all,

I am working with the ST25R3911B discovery board (ST25R3911B-DISCO) and am attempting to directly interface the ST25R3911B IC with an Atmel microcontroller (in this case, and Arduino Uno).

Over SPI, I can read and write the registers of the ST25R3911B with no issues, I can even send direct commands. The ST25R3911B reacts/responds to my actions as I would expect it to.

The issue I have ran into is that I am simply unable to read or write to the FIFO. This is confusing because, in principle, it is a very similar operation to reading/writing the register. The only difference to the microcontroller is that the Mode Bits and 'trailer' it transmits are different. Refer to page 33 of the ST25R3911B to take a look at that detail.

After trying to write to the FIFO, the 'FIFO Status Register 1' (refer to page 97) does not change; it always reads zero. This indicates that I did not actually write anything to the FIFO.

Further, after trying to read the FIFO, bit 6 of the 'FIFO Status Register 2' does not change (nor does bit 5, not that it should though). This indicates that no data was actually read from the FIFO.

So I can't read or write to the FIFO, but registers and direct commands are fine. Due to this, I don't think my problem involves my SPI settings or my microcontroller.

I think it could be two things:

  1. There is a detail in the spec sheet I missed, such as a config register that needs to be written before interacting with FIFO
  2. Something else on the discovery board is interfering, I say this because I had to solder (permanently close) the reset button to the STM32 included on my discovery board. I believe the STM32 on the discovery board handles the serial communication when you connect the board to a PC over micro-usb. I don't need that so I keep it sleeping; otherwise the STM32 seems to automatically communicate over SPI to the ST25R3911B and my microncontroller can't talk to the ST25R3911B. But why wpuld a supposed interference only affect FIFO? I don't think it is the case.

Any ideas what might be behind this?

Thanks much,

Simon R.

This topic has been closed for replies.
Best answer by Grégoire Poulain

Hi Simon,

If you use the direct command Write FIFO with a certain number of bytes this will be reflected on the fifo_b bits (FIFO Status Register).

The other bits you mentioned fifo_unf and fifo_ovr, will only be affected when the FIFO underflows/overflows during transmission/reception.

To verify your communications you should be able to write to the FIFO n bytes, check the FIFO Status register, and then retrieve the same bytes with a Read FIFO command.

From your description it seems a SPI issue. Please verify the SPI signals and check that the Chip Select line is OK.

Perhaps if you add a SPI trace we can better support you.

Kind regards

GP

2 replies

Grégoire Poulain
ST Employee
August 31, 2018

Hi Simon,

If you use the direct command Write FIFO with a certain number of bytes this will be reflected on the fifo_b bits (FIFO Status Register).

The other bits you mentioned fifo_unf and fifo_ovr, will only be affected when the FIFO underflows/overflows during transmission/reception.

To verify your communications you should be able to write to the FIFO n bytes, check the FIFO Status register, and then retrieve the same bytes with a Read FIFO command.

From your description it seems a SPI issue. Please verify the SPI signals and check that the Chip Select line is OK.

Perhaps if you add a SPI trace we can better support you.

Kind regards

GP

Simon R.
Simon R.Author
Associate
January 3, 2019

Hi all,

I have finally revisited this issue after a few months away from it, and I found the actual solution to my problem within five minutes of returning to it. It was painfully obvious: bit 7 ('en') of the the Operation Control Register must be set to 1. Now the FIFO can be read and written to as expected.

Thanks much!