cancel
Showing results for 
Search instead for 
Did you mean: 

CRC Polynomial

Mjohn.1
Associate

Hi,

How to calculate the ISO14443-a CRC value(16 bit). Please help me how to get the CRC.

ISO14443-A >>> CR95HFDLL_SENDRECEIVE, 300028

<< 8015 6A1E4DB17E00004B3592000000000000 9BC3 080000

0x9BC3 ISO14443-a CRC value

Kind Regards,

Merin

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
alister
Lead
4 REPLIES 4
alister
Lead

A Google search threw these...

A CRC function and links to others: https://stackoverflow.com/questions/40869293/iso-iec-14443a-crc-calcuation

Some details on CR95HF and clues where to get more: https://community.st.com/s/question/0D50X00009XkW7G/iso-14443a-cr95hf-and-the-crc-bit

Another CRC implementation: https://www.microchip.com/forums/m896426.aspx

Datasheets, tools and software: https://www.st.com/en/nfc/st25-nfc-rfid-tags-readers.html

Mjohn.1
Associate

The resolved program to calculate the ISO14443-a CRC value(16 bit) as follow.

data_byte = 0x12;

CHECKSUM_CALCULATE(0x12 ^ 0x6363);

unsigned int CHECKSUM_DATA;

void CHECKSUM_CALCULATE(unsigned int C_DATA)

{

unsigned int n;

 for(n=1;n<=8;n++)

 {

 if((C_DATA & 0x01)==0x01)

 {

 C_DATA = C_DATA >> 1;

 C_DATA = C_DATA ^ 0x8408;

 }

 else

 {

 C_DATA = C_DATA >> 1;

 }

 }

 CHECKSUM_DATA = C_DATA;

}

ISO14443A Polynomial is 0x8408, initial value is 0x6363, CRC output is 0x626d

online 16bit crc calculator : https://hub.zhovner.com/tools/nfc/

Kind Regards,

Merin

Brian TIDAL
ST Employee

Hi,

just for my curiosity, why do you need to compute the CRC? The CR95HF does the job for you and provides a CRC error bit in the response flags of the SendReceive command.

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

The CRC here is 0xC39B in small endian form. If you run the data+crc thru the right shifting algorithm the data will divide cleanly resulting in a zero remainder.

C:\MSVC\CRC>iso14443a

626D == 0x626D

626D

test_one=C39B << Note High/Low bytes swapped

test_two=0000

PASS

// ISO14443A CRC Example   sourcer32@gmail.com
 
#include <windows.h>
#include <stdio.h>
#include <stdlib.h>
 
typedef unsigned char uint8_t;
typedef unsigned short uint16_t;
typedef unsigned long uint32_t;
 
uint16_t crc_iso14443a(uint16_t crc, uint8_t data)
{
  int i;
  crc = crc ^ data;
  for(i=0; i<8; i++)
    if (crc & 1)
      crc = (crc >> 1) ^ 0x8408;
    else
      crc >>= 1;
  return(crc);
}
 
uint16_t crc_iso14443a_quick(uint16_t crc, uint8_t data)
{
  static const uint16_t crctbl[] = { // 0x8408 Nibble Table, sourcer32@gmail.com
    0x0000,0x1081,0x2102,0x3183,0x4204,0x5285,0x6306,0x7387,
    0x8408,0x9489,0xA50A,0xB58B,0xC60C,0xD68D,0xE70E,0xF78F };
 
  crc = crc ^ data;
 
  crc = (crc >> 4) ^ crctbl[crc & 0xF]; // Two rounds of 4-bits
  crc = (crc >> 4) ^ crctbl[crc & 0xF];
 
  return(crc);
}
 
uint16_t crc_iso14443a_quick_block(uint16_t crc, int size, uint8_t *buffer)
{
  while(size--)
    crc = crc_iso14443a_quick(crc, *buffer++);
 
  return(crc);
}
 
void test_one(void)
{
  // ISO14443-A >>> CR95HFDLL_SENDRECEIVE, 300028
  // << 8015 6A1E4DB17E00004B3592000000000000 9BC3 080000
 
  uint8_t data[] = {
    0x6A,0x1E,0x4D,0xB1,0x7E,0x00,0x00,0x4B,
    0x35,0x92,0x00,0x00,0x00,0x00,0x00,0x00 };
 
  uint16_t crc;
 
  crc = crc_iso14443a_quick_block(0x6363, sizeof(data), data);
 
  printf("test_one=%04X\n", crc );
}
 
void test_two(void)
{
  // ISO14443-A >>> CR95HFDLL_SENDRECEIVE, 300028
  // << 8015 6A1E4DB17E00004B3592000000000000 9BC3 080000
 
  uint8_t data[] = {
    0x6A,0x1E,0x4D,0xB1,0x7E,0x00,0x00,0x4B,
    0x35,0x92,0x00,0x00,0x00,0x00,0x00,0x00,
    0x9B,0xC3 };
 
  uint16_t crc;
 
  crc = crc_iso14443a_quick_block(0x6363, sizeof(data), data);
 
  printf("test_two=%04X\n", crc);
  if (crc == 0) puts("PASS"); else puts("!!FAIL!!");
}
 
int main(int argc, char **argv)
{
  printf("%04X == 0x626D\n", crc_iso14443a(0x6363, 0x12) );
 
  printf("%04X\n", crc_iso14443a_quick(0x6363, 0x12) );
 
  test_one();
  test_two();
 
  return(1);
}

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..