cancel
Showing results for 
Search instead for 
Did you mean: 

CR95HF FAST_READ Command using NTAG213 (14443A)

TGree.2
Associate

We are using the CR95HF over SPI and communicating with a single NTAG213 tag.

I can successfully configure the reader and read 4 pages of user memory reliably using the READ command:

00 04 03 30 04 28. // Reads 16 bytes from Addr 0x04

We would like to read multiple blocks using the FAST_READ command but the following command structure gives an 0x87 error;

00 04 04 3A 04 07 28

Any idea why this doesn't work?

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Brian TIDAL
ST Employee

Hi,

I've tried the 04 04 3A 04 07 28 command on my side and I've received:

80 15 30 30 30 30 32 38 FF FF 06 FF FF FF 07 FF FF FF A4 A5 08 00 00

Can you check the Frame Delay Time in your protocolSelect command? It should be at least T_ACK/NACK (see the Tag Datasheet).

See also https://community.st.com/s/question/0D50X0000AFqKjkSQF/why-does-my-cr95hf-respond-with-0x87-timeout-or-no-tag-after-successfully-writing-to-a-ntag216-nfc-forum-type-2-compliant-tag

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
Brian TIDAL
ST Employee

Hi,

I've tried the 04 04 3A 04 07 28 command on my side and I've received:

80 15 30 30 30 30 32 38 FF FF 06 FF FF FF 07 FF FF FF A4 A5 08 00 00

Can you check the Frame Delay Time in your protocolSelect command? It should be at least T_ACK/NACK (see the Tag Datasheet).

See also https://community.st.com/s/question/0D50X0000AFqKjkSQF/why-does-my-cr95hf-respond-with-0x87-timeout-or-no-tag-after-successfully-writing-to-a-ntag216-nfc-forum-type-2-compliant-tag

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
TGree.2
Associate

The increased T_ACK helped - thank you!

Regards

Tony