Skip to main content
duncan
Associate II
December 23, 2013
Solved

communicating with the CR95HF discovery without using the DLL

  • December 23, 2013
  • 1 reply
  • 856 views
Posted on December 23, 2013 at 13:06

I have managed to do what I want with this board using the DLL, however I want to expand my use of the board to other operating systems such as Linux and OSX (for Mac) and these do not use DLLs. Is there any way to communicate with the board using something other than the downloadable DLL? I have looked through the documentation, but I do not understand really from that how to access the board if it is outlined in there, so I would need some extra help. My email address if you need is turmunder AT gmail DOT com. Alternatively, if it is possible to make the source code for the DLL itself available, then I could try reverse engineering that to do what I want.

#cr95hf-osx-linux-arm
This topic has been closed for replies.
Best answer by Anais GALLIGANI
Posted on January 23, 2014 at 15:16

Hello,

Good news, 

We are  proposing only  windows dll for now.

We will be interest per your Linux & Mac version when they are available.

ST NFC/RFID Dynamic support

1 reply

Anais GALLIGANI
Anais GALLIGANIBest answer
Visitor II
January 23, 2014
Posted on January 23, 2014 at 15:16

Hello,

Good news, 

We are  proposing only  windows dll for now.

We will be interest per your Linux & Mac version when they are available.

ST NFC/RFID Dynamic support