2024-06-12 6:38 AM
Hi,
We have designed a board based on ST25R3911B and it is about to be tested by a Notified Body with regards to RED/EMC.
In relation to this, I am wondering if there is ready-made SW available, that can be used for setting the radio to transmit a single tone on a given channel? It is needed as part of the RED-testing.
Br,
Chato
Solved! Go to Solution.
2024-06-12 7:28 AM
Hi Chato,
not exactly sure about your question. NFC is 13.56MHz only - no different channels available. Emitting a "tone": Just enable the field.
Or do you have different requirements?
BR, Ulysses
2024-06-12 7:28 AM
Hi Chato,
not exactly sure about your question. NFC is 13.56MHz only - no different channels available. Emitting a "tone": Just enable the field.
Or do you have different requirements?
BR, Ulysses