2023-03-22 8:10 AM
Extract from your user manual:
Introduction
The STSW-EV-VNF1048F is the graphical user interface (GUI) dedicated to set and control the EV-VNF1048F using an EVSPC582B programmed with a specific firmware able to create an advanced controller for a MOSFET in high side configuration, designed for the implementation of an intelligent high side switch for 12 V, 24 V and 48 V automotive applications.
2024-09-30 4:19 AM
I have the same problem. Can not find the "dedicated software" for the Eval board. I wonder why they choose that expensive EVSPC582B board instead of using a cheaper and more convenient Nucleo board with STM32?
It would be much simpler if they provide a SPI Library for the VNF1048F.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.