cancel
Showing results for 
Search instead for 
Did you mean: 

What should be the voltage accross VBAT+ and VBAT- of M4Z32-BR00SH1 battery at the time of purchase. If it is zero at the time of purchase, can it be recharged?

JDHOP.1
Associate
 
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

Welcome, @JDHOP.1​, to the community!

The voltage between both terminals should be nominally 2.8V, below 2.0V it should be considered discharged.

The battery is based on lithium carbon monofluoride chemistry and is not rechargeable.

Does it answer your question?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

3 REPLIES 3
Peter BENSCH
ST Employee

Welcome, @JDHOP.1​, to the community!

The voltage between both terminals should be nominally 2.8V, below 2.0V it should be considered discharged.

The battery is based on lithium carbon monofluoride chemistry and is not rechargeable.

Does it answer your question?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Dear Peter,
Yes, you have answered my question.
Thanks a lot!
With regards,
J B Dhopte

Great!

If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.