cancel
Showing results for 
Search instead for 
Did you mean: 

What is differences between L6235 and L6229 (driver for 3-phase BLDC motor)

rwojtanowski
Associate
Posted on June 14, 2007 at 09:46

What is differences between L6235 and L6229 (driver for 3-phase BLDC motor)

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
rwojtanowski
Associate
Posted on May 17, 2011 at 10:14

What is differences between L6235 and L6229 (driver for 3-phase BLDC motor) - only output current ?

I want to drive 3-phase bldc motor ( 1A max output current, 120° Hall efect decoding logic) - It really doesn't mater which chip I will use ?

vincenzo1
Associate II
Posted on May 17, 2011 at 10:14

The only difference is the size of integrated power mosfets (i.e. maximum current). Choosing between L6235 and L6229 and the package type (SO, PowerDIP, PowerSO) take into account power dissipation more than rated current (see datasheet and app.notes).

Regards

Vincenzo MARANO

STMicroelectronics