2026-04-22 1:29 AM - last edited on 2026-05-08 5:34 AM by Peter BENSCH
[Moderation] Separated from the previous thread, as the STEVAL-ISV019V1 is a different topic.
Hi,
As the questioner mentioned, the voltage measured on the STORE pin is about 2.416V. Should we charge the battery at this time? What conditions can raise the voltage of STORE to VEOC.
Thank you for your reply and your help.
2026-04-22 7:38 AM
Welcome @HUANG2, to the community!
Important is:
VSTORE only rises sufficiently if more energy is supplied to the storage capacitor or the STORE node than is drawn from it, for example by:
Check:
As long as VSTORE does not reach VEOC, LDO2 remains off. The battery is not meaningfully enabled in this state. Only when STORE rises above the EOC threshold through sufficient energy input does the internal pass transistor close.
Regards
/Peter
2026-05-06 11:59 PM - last edited on 2026-05-07 2:06 AM by Peter BENSCH
The ST Community moderator has translated the post to comply with the language of the Community which is English. For more information, see: ST Community Terms and Conditions - STMicroelectronics Community
Hello,
I purchased the STEVAL-ISV019V1 evaluation board. After connecting the solar panel, the VSTORE voltage reached the EOC threshold, and the LDO2 output voltage was also normal and stable at 3.3V. However, when I used LDO2 to power the sensor node, the VSTORE voltage dropped and the LDO2 output voltage fell to 1.2V. After that, I disconnected the load and measured the VSTORE voltage at 2.881V. However, the VSTORE voltage did not rise again for a long time. What could be causing this? Is it possible that the chip is damaged, or that another component has failed?
My solar panel open-circuit voltage is between 2.8V and 3.4V.
Thank you for your reply and help.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.