2011-09-22 8:08 AM
Hi I have one new project for my application and I have used the Viper53-E (dip8) to build a small SMPS AC/DC. After the selection of components with the VIPER SOFTWARE, I have build the SMPS, but don't have the correct voltage in output.
In the attached file the electric drawing and the data of transformer. In the out I have 50V not I have reduced the secondary winding at 10 turn, but the output voltage don't change why? Best Regards Daniele2011-09-23 3:15 AM
Hi Daniele,
You can try to use the secondary regulation and I would consider the switching frequency. I think, the 300kHz is not optimal. The 100kHz would be more suitable. Best regards Jakub2011-09-23 4:53 AM
Thanks Jakub,
I have verified the switching frequency this morning and is 100kHz.I
further modified
the number
of turns
of the secondary
from 22 to
8 turns
to lower
the output voltage
and
now I'm
changing the
transformer turns
ratios
to further improve
the operation
. Daniele